AnsweredAssumed Answered

RM0394 reference manual Errors

Question asked by Dave Jones on Apr 6, 2018
Latest reply on Apr 9, 2018 by Imen D

For the next update to RM0394 ("Reference Manual - STM32L43xxx STM32L44xxx STM32L45xxx STM32L46xxx
advanced ARM®-based 32-bit MCUs"):

 

=========

On page 74, in the table showing page locations in memory, it shows page 255 being at location:

0x087F F800 - 0x087F FFFF

 

That should be:

0x0807 F800 - 0x0807 FFFF

 

==========

At the top of page 81, in the steps for "Mass Erase" (title is on previous page), step 4 is:

 

4. Set the STRT bit in the FLACH_CR register.

 

it should be:

 

4. Set the STRT bit in the FLASH_CR register.

 

==========

On page 81, in the steps involved in "Standard Programming", step 7 is:

 

7. Clear the PG bit in the FLASH_SR register if there no more programming request
anymore.

 

It should be:

 

7. Clear the PG bit in the FLASH_CR register if there no more programming request
anymore.

 

=========

On page 82, in the steps for Fast Programming, step 8 is:

 

8. Clear the FSTPG bit in the FLASH_SR register if there no more programming request
anymore.

 

It should be:

 

8. Clear the FSTPG bit in the FLASH_CR register if there no more programming request
anymore.

Outcomes