AnsweredAssumed Answered

STM32F412 UART Boot no response ...

Question asked by Eryk Sokolowski on Apr 6, 2018
Latest reply on Apr 9, 2018 by Eryk Sokolowski

Hi There,

 

I am going a bit crazy about this. I have a custom board with STM32412 on it. 

 

I have connected TX and RX to PA9 and PA10, I ensure that Boot0 == 1 and PB2 (boot1) == 0 (just in case). As per  AN2606.

 

And the board doesn't respond to 0x7F.

 

The same setup with the NUCLEO evaluation board works fine! I use a UM232R @ 3v3 both TX and RX are pulled up internally

 

What am I missing?

 

The MCU on the board was tested in its virgin state ( from the box ) and also after programming using JTAG to check if it works?

 

Any clues or pointer would be much appreciated?

Outcomes