AnsweredAssumed Answered

STM32H7 SPI ISSUE

Question asked by maheshwar reddy on Apr 6, 2018
Latest reply on Apr 6, 2018 by Clive One

Hai, Iam using the STM32H743VIT controller , We are using the spi4 in our board ,we generated the code using the cube mx  nothing is coming (CLK and SIN)when transmit the data using the function ( HAL_SPI_Transmit(SPI_HandleTypeDef *hspi, uint8_t *pData, uint16_t Size, uint32_t Timeout)). we configured the SPI to the 8 bit mode.But with the same configuration the SPI2 is working fine.  

Thank you 

Best regards 

Maheshwar.

Outcomes