AnsweredAssumed Answered

Cubemx 4.25 STM32F767 EXTI problem

Question asked by Peter Mather on Apr 3, 2018
Latest reply on May 3, 2018 by Andrei Chichak

I've configured a number of pins on the 767 as EXTI but there is no option in NVIC to enable the interrupts and no code generated. The pins are correctly identified in  the GPIO configuration tab.

 

Moreover, the example for Nucleo-767ZI uses pin PC13 which the cube pinout dropdown says is EXTI13 but the example code treats as EXTI_Line15_10

 

Is this simply a bug/omission in CubeMX or am I missing something as usual?

Attachments

Outcomes