AnsweredAssumed Answered

Can I have a PWM 5V logic signal coming into L9907?

Question asked by Tom B on Apr 3, 2018
Latest reply on Apr 6, 2018 by Stefano Cini

The L9907 datasheet states that I/O is 3.3V logic compatible.  It also states that I/O pins can withstand voltages up to 35V in the 'Absolute Maximum Ratings' section on page 17.  I was wondering if it were wise to have a PWM 5V logic signal coming into the L9907 3-Phase Gate Driver interfacing with 5V PWM from MCU.

Outcomes