AnsweredAssumed Answered

STM32H743i & stmpe811

Question asked by greenwood.greg on Mar 31, 2018
Latest reply on Apr 2, 2018 by greenwood.greg

I am trying to construct a CubeMX based version of the LwIP_HTTP_Server_Netconn_RTOS project in the repository.  I have used the board selector in CubeMx of the H743i-Eval and setup the options for the hardware to match with the example.  I have added the same drivers and BSP components as used in the project and all compiles OK.

However as soon as I try to add the call BSP_LCD_Init() the linker throws numerous errors all coming from stmpe811.o flagging IOE_Read, IOE_Write, IOE_Delay, IOE_ReadMultiple, IOE_ITConfig as undefined references.

What is going on?

I have attached the eclipse based project.

Attachments

Outcomes