AnsweredAssumed Answered

STM32 HAL RCC ClockConfig Hard Fault at >65°C

Question asked by schweizer.roger on Mar 26, 2018
Latest reply on Mar 26, 2018 by Clive One

Hi

I have following Problem:

 

At <65 °C ambient temperature and PowerOff-On.
My STM32f373 works fine.

At> 65 ° C ambient temperature and PowerOff-On

I get a HardFault Error at the following function:

 

void SystemClock_Config(void)
{

 .............

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
  {
    _Error_Handler(__FILE__, __LINE__);
  }

  ............
}

 

What is wrong?

Can someone help me ?

 

Kind regards

Roger

Outcomes