AnsweredAssumed Answered

LL driver not supported ??? [ CubeMX 4.22.1 with STM32F4]

Question asked by Jems On on Mar 26, 2018
Latest reply on Mar 26, 2018 by Jems On

Hi,

 

I am currently using version 4.22.1 of MX cube with a F4 board. I want to use the interface of CubeMX to initialize a device (in this case I2C) but using LL driver. As describe  on the UserManual UM1718 :

 

 

In my project setting> advanced setting. I do not have a column allowing me to validate or not visibility (static) Similarly I only have the option HAL which can be chosen if I click in the driver selector part ...



I can  add the LL library to my project manually, but I would like to know if I'm doing something wrong with Cube MX.

 

Thanks in advance

 

Jems

Outcomes