AnsweredAssumed Answered

ERROR REPORT - STM32H7x3 Reference manual : GPIO MODER

Question asked by Julien FAUCHER on Mar 23, 2018
Latest reply on Mar 26, 2018 by Nesrine M

Hi,

 

In the reference manual for the STM32H7x3 RM (RM0433) the register map for the GPIO in the GPIO register map (p.500) appear to be incorrect :

  • For the GPIOA, based on H7 Headers it's actually MODERx and not MODEx
  • For GPIOx : There is that "MODEv1" bit which is also false (MODER).

Then, those three rows may be merged into one single row (excepted that the initial values aren't the same)

 

Best regards,

Julien FAUCHER#

Outcomes