AnsweredAssumed Answered

USB Connection for STM32F072C8T6

Question asked by Justin Kim on Mar 19, 2018
Latest reply on Mar 20, 2018 by waclawek.jan

Hello,

 

I saw in the datasheet that the max USB voltage input for the STM32F072C8T6 is approximately 3.6 V. Since the USB data voltage can go up to 5 V, I was wondering how one would make the connection between the USB to this MCU. If a voltage translator is required, could you please recommend one for this MCU?

 

Or, am I incorrect and you can get away with just directly connecting the USB to the MCU USB data lines?

 

Thank you.

Outcomes