AnsweredAssumed Answered

GSM library for Contiki OS on STM32F411RET6

Question asked by Aishwarye Chauhan on Mar 19, 2018
Latest reply on Mar 20, 2018 by Aishwarye Chauhan

Hello,

 

I've integrated the following GSM library(with some changes) ,along with eclipse_paho_MQTT device client on STM32F411RET6. I'm using a SIMCOM 7100E LTE module for communication with the cloud (on the gateway side ) and STM spirit1 modules for communication with the nodes. The RTOS I'm currently using is FreeRTOS for managing threads and synchronizing between them.

Now, I want to integrate this with Contiki OS as we have a working 6lowPAN mesh over subGHZ implemented using Contiki's 6lowPAN stack. Although it will be trivial to do so, I still wanted to know a few things :

  1. Is using the aforementioned GSM library the recommended approach.
  2. Are there any alternatives to the above library that might be more popular?
  3. Is Contiki a better solution for STM32F4xx series or should I be using FreeRTOS, any other RTOS ?

 

The current use-case is Smart Street Lighting so availability of power is not an issue, however we would like to extend it to other use-cases where conserving power might be needed.

 

Thanks,

Aishwarye Chauhan

Outcomes