AnsweredAssumed Answered

WiFi VCOM Example Not Working

Question asked by Drake Miller on Mar 10, 2018

Hi, 

   I just purchased the following setup:

Computer: i7 / Windows 10

Nucleo: STM32F401

Expansion: IDW04A1

I have Trustudio as the compiler currently. Updated drivers to current.  

 

My problem is that when working the hands-on tutorial I can not get past the VCOM example.

 

I drop the Project.bin into the Nucleo board per the instructions open a terminal window and get only garbage output from the Wifi module. The blue LED2 is flashing and the others are solid (LED1 and LED4).  

 

I am stuck and not sure how to proceed if I can't get the module to work with this simple example. 

 

Thank you in advance for any insights here. 

 

Drake

Outcomes