AnsweredAssumed Answered

ST-LINK/V2-1 software

Question asked by Jeroen de Bruijn on Mar 8, 2018
Latest reply on Mar 11, 2018 by brown.geoffrey.001

I'm designing a PCB and am interested in adding the ST-LINK/V2-1 programming and debugging board to it. I found the schematics and example PCB design in the Nucleo F103RB page but could not find the software anywhere. I know I can just buy the components used in the design, but then the STM32F103CBT6, used in the ST-LINK/V2-1 section, would be unprogrammed (or only contain a bootloader). The program that is used to do the SWD/JTAG interface between the host MCU needs to be programmed to it (using USB and bootloader or ST-LINK/V2 or something), but I don't have that software. Is that software available anywhere? I could only find the STSW-LINK007 firmware update so far. Preferably I'd like the source code of the software so it doen't matter if I swap any pins in the design or add some LEDs and extra signals to the host MCU or something.

Really hope someone (from ST) can help we with this!

Outcomes