AnsweredAssumed Answered

Bluenrg-ms get accepted connection interval

Question asked by Chalk Talk on Mar 6, 2018
Latest reply on Mar 9, 2018 by Antonio Vilei

Hi, I'm looking to do some timing specific code with the Bluenrg MS

It is running as a peripheral, and once a connection is established, we send an update connection request to the master, and get a response saying is was accepted.

 

The problem I'm running into, is what is the exact connection interval the master will use?

In the request we supply a min and max value (10ms to 20ms, 0 slave latency), but the response only says that these parameters were accepted.

 

Is there a procedure, or ACI type command that we can use to query the connection interval actually being used?

Outcomes