AnsweredAssumed Answered

STM32L475 USB OTG Host GPIO Interrupt Failed

Question asked by Brian Dahl on Mar 2, 2018
Latest reply on Mar 3, 2018 by waclawek.jan

Hi,

i have a STM32L475 with USB OTG as Host with USB Disk attached and an GPIOInt with callback void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin).

 

If i build my HAL without USB all is ok, but when i build it with USB Support, the callback is never called anymore.

 

Can anybody help me (I have tested to set the usb Priority to 1 and the GPIOInt to 0 but it had failed).

 

Best Regards

Brian

Outcomes