AnsweredAssumed Answered

LISD2E12 INT1_THS not changing tilt threshold

Question asked by Joseph Lehman on Feb 23, 2018
Latest reply on Apr 13, 2018 by Joseph Lehman

The INT1_THS register value does not seem to change the threshold at which an event is triggered. I can read and write the INT1_THS(0x32) so I know my writes are working. I poll the INT1_SRC register and watch the bits change so the position enable ints are working it is just that the threshold seems fixed not adjustable.

 

INT1_CFG = 0xCF to enable X & Y position triggering

INT1_THS = 0x20 = 0.5g or 30 degrees.  (actual int flags trip around 0.94g/66 degrees)

 

Thanks in advance for any help.

Outcomes