AnsweredAssumed Answered

BUG: STM32F446 timers on APB1 run faster than indicated in Cube and datasheet

Question asked by ramakers.andre on Feb 21, 2018
Latest reply on Feb 23, 2018 by ramakers.andre

Hi all,

 

We use the STM32F446 for a new project. We noticed that the clock for the timers on the APB1 is x4 instead of x2 when the APB1 prescaler is not equal to 1. 

 

In our test we have used a system clock of 168MHZ and APB1 prescaler /4 which gives 42MHz. Cube says that the APB1 timer clock is 84MHz but my output signals on the timers are twice as fast. We have checked the 42MHz on the other APB1 peripherals with UART5, there the timing is correct.

 

Please udate the reference manual and the Cube for this device.

 

And maybe also indicate that the USB peripheral for this device is like the F7 USB core...

 

Thanks,

André

Outcomes