AnsweredAssumed Answered

STM32CubeMX (STM32F373) Initialization ADC + SDADC problem ?

Question asked by davydenko.sergey on Oct 22, 2014
The generated code contains an additional fragment, which gives a compilation error
Мy cube project attached...

Сode:
void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)
{


  GPIO_InitTypeDef GPIO_InitStruct;
  if(hadc->Instance==ADC1)
  {
  /* USER CODE BEGIN ADC1_MspInit 0 */


  /* USER CODE END ADC1_MspInit 0 */
    /* Peripheral clock enable */
    __ADC1_CLK_ENABLE();
  
    /**ADC1 GPIO Configuration    
    PA0     ------> ADC1_IN0
    PA1     ------> ADC1_IN1
    PA4     ------> ADC1_IN4
    PA5     ------> ADC1_IN5 
    */
    GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_4|GPIO_PIN_5;
    GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);


    /* Peripheral DMA init*/
  
    hdma_adc1.Instance = DMA1_Channel1;
    hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
    hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
    hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
    hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
    hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
    hdma_adc1.Init.Mode = DMA_NORMAL;
    hdma_adc1.Init.Priority = DMA_PRIORITY_LOW;
    HAL_DMA_Init(&hdma_adc1);


    __HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1);


    hdma_sdadc1.Instance = DMA2_Channel3;
    hdma_sdadc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
    hdma_sdadc1.Init.PeriphInc = DMA_PINC_DISABLE;
    hdma_sdadc1.Init.MemInc = DMA_MINC_ENABLE;
    hdma_sdadc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
    hdma_sdadc1.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
    hdma_sdadc1.Init.Mode = DMA_NORMAL;
    hdma_sdadc1.Init.Priority = DMA_PRIORITY_LOW;
    HAL_DMA_Init(&hdma_sdadc1);


    __HAL_LINKDMA(hadc,hdma,hdma_sdadc1);


  /* USER CODE BEGIN ADC1_MspInit 1 */


  /* USER CODE END ADC1_MspInit 1 */
  }


}

void HAL_ADC_MspDeInit(ADC_HandleTypeDef* hadc)
{


  if(hadc->Instance==ADC1)
  {
  /* USER CODE BEGIN ADC1_MspDeInit 0 */


  /* USER CODE END ADC1_MspDeInit 0 */
    /* Peripheral clock disable */
    __ADC1_CLK_DISABLE();
  
    /**ADC1 GPIO Configuration    
    PA0     ------> ADC1_IN0
    PA1     ------> ADC1_IN1
    PA4     ------> ADC1_IN4
    PA5     ------> ADC1_IN5 
    */
    HAL_GPIO_DeInit(GPIOA, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_4|GPIO_PIN_5);


    /* Peripheral DMA DeInit*/
    HAL_DMA_DeInit(hadc->DMA_Handle);
    HAL_DMA_DeInit(hadc->hdma);
  /* USER CODE BEGIN ADC1_MspDeInit 1 */


  /* USER CODE END ADC1_MspDeInit 1 */
  }


}

Attachments

Outcomes