AnsweredAssumed Answered

STM32Cube_FW_H7_V1.2.0 Bugs - NUCLEO HSE_VALUE

Question asked by Clive One on Feb 15, 2018
Latest reply on Apr 23, 2018 by Clive One

STM32Cube_FW_H7_V1.2.0\Projects\STM32H743ZI-Nucleo\Applications\FatFS\FatFS_uSD_Standalone\Inc\stm32h7xx_hal_conf.h

 

\STM32Cube_FW_H7_V1.2.0\Projects\STM32H743ZI-Nucleo\Applications\LwIP\LwIP_HTTP_Server_Netconn_RTOS\Inc\stm32h7xx_hal_conf.h

 

Nucleo uses 8 MHz HSE in BYPASS mode, the wrong HSE_VALUE breaks USART, rate computations, etc

 

/**
  * @brief Adjust the value of External High Speed oscillator (HSE) used in your application.
  *        This value is used by the RCC HAL module to compute the system frequency
  *        (when HSE is used as system clock source, directly or through the PLL).
  */
#if !defined  (HSE_VALUE)
#define HSE_VALUE    ((uint32_t)25000000) /*!< Value of the External oscillator in Hz   */
#endif /* HSE_VALUE */

Outcomes