AnsweredAssumed Answered

[F767ZI] Sampling and storing Measurement Data

Question asked by Armin L. on Feb 16, 2018
Latest reply on Feb 27, 2018 by Armin L.

Hello!

 

I want to start a project with the NUCLEO-F767ZI soon. In this project I want to measure some quantities with up to 100 kSamples/s and store the data.
Would it be physically possible to have the data either stored to an SD memory card (via SDMMC interface) or sent via Ethernet with up to 10 MB/s in realtime and still having some computing power to execute additional calculations on the MCU? Or are there restrictions on the achievable data rates?
And which memory device or data transfer protocol would you suggest for that purpose in general?

 

Thanks in advance!

Outcomes