AnsweredAssumed Answered

Serial over ST-Link USB on stm32F722

Question asked by David Pekin on Feb 14, 2018
Latest reply on Feb 15, 2018 by David Pekin

Hello,

 

I've developed a program reading and writing serial data using USART6 and pins 6 & 7 on GPIOC.  It uses DMA to perform the RX & TX and is working fine.  We thought we might be able to save some wiring effort if we could use the ST-Link serial port on the USB so I changed USART6 to USART3 and the tx rx pins to 8/9 on GPIOD.  I also changed the baud rate way down to 9600 for testing. 

 

Unfortunately this "simple" change did not work.  When I send a serial command to the ST-Link serial port, the program has a catastrophic failure and ends in an exception.  The transmit and receive callbacks are never fired.

 

Is there some limitation on the use of the ST-Link serial channel that prevents this?  Also, the failure occurs whether the debugger is running or not.

 

Thanks for any insight here.

Outcomes