AnsweredAssumed Answered

STM32F071V8 ADC ADC_IN17 (VREFINT) measurement errors

Question asked by Sandhya Sharma on Feb 14, 2018
Latest reply on Feb 16, 2018 by Sandhya Sharma

Hi all,

 

We are using a STM32F071V8 MCU in our project. I am polling the ADC to read the data and have followed the following procedure to initialize the ADC:

1. enable clock to respective GPIOs
2. Initialize GPIO pins as Analog Inputs

3. Turn on HSI14MHZ clock
4. enable clock going to ADC
5. reset ADC
6. begin ADC calibration
7. wait for calibration to finish 
8. enable the ADC
9. enable the VBAT divider and temperature sensor
10. Configure the sampling time
11. Configure ADC_CFGR1  register for settings - 12 bit resolution; Analog WDT disabled; Sinlge conversion mode
12. Configure ADC_CFGR2  register for settings - ADCCLK (Asynchronous clock mode)
13. wait for ADC to finish starting up

 

I was trying to determine the value of VDDA by using the formula below: 

VDDA = 3.3 V x VREFINT_CAL / VREFINT_DATA

 

The VREFINT_CAL value read is 1519. Upon reading the ADC_DR register after calibration I found the calibration factor to be 0x42. 

When I poll for the data on the ADC_IN17 channel it varies drastically with respect to the sampling time.

 

Please find the results below: 

SMP[2:0] = 000: 1.5 ADC clock cycles ; ADC counts = 1891; VDDA = 2.26V 

                   001: 7.5 ADC clock cycles ; ADC counts = 1657; VDDA = 3.06V

                   010: 13.5 ADC clock cycles;ADC counts = 1383; VDDA = 3.6V (Worse!)

                   011: 28.5 ADC clock cycles;ADC counts = 1510; VDDA = 3.319V 

                   Remains almost same for higher sampling time.

 

Could you please help me draw an inference here?

 

Thanks in advance. 

 

 

Outcomes