AnsweredAssumed Answered

STM32Cube_FW_L0_V1.10.0 versus STM32CubeExpansion_NFC2_V1.1.0 HAL library

Question asked by christophe trichet on Feb 8, 2018

Hello,

i use for STM32L053, the STM32CubeExpansion_NFC2_V1.1.0 (extension of NFC2) writeURI project;

i want to add to this project ADC + RTC + Watch-dog

 

Where should i shearch the HAL files for these modules : should i use

#

STM32Cube_FW_L0_V1.10.0 HAL library or the

STM32CubeExpansion_NFC2_V1.1.0 HAL library

?

 

The files are not the same under

-Repository\STM32Cube_FW_L0_V1.10.0\Drivers\STM32L0xx_HAL_Driver

-or Repository\STM32CubeExpansion_NFC2_V1.1.0\Drivers\STM32L0xx_HAL_Driver

 

Thanks for any answer

best regards

Outcomes