AnsweredAssumed Answered

Frequency and channel setting of SPIRIT1 for 400-406MHz

Question asked by Srikanth Govindavajjala on Feb 7, 2018
Latest reply on Feb 16, 2018 by Srikanth Govindavajjala

Hello,

 

I want to operate the SPIRIT1 in the frequency range of 400 MHz to 406 MHz. And channel spacing of 200KHz. That means my first frequency is 400.2 MHz and if i want to go for the next frequency it could be 400.4 MHz and so on.  Can anyone send me the Synthesizer setting values and what Crystal has to be used to operate in the frequency range.

 

Thanks,

Srikanth

Outcomes