AnsweredAssumed Answered

STM32-MAT-TARGET Can not find which APB timer TIM1 is connected to.

Question asked by antonio rueda on Feb 4, 2018
Latest reply on Feb 6, 2018 by Sebastian K.

Hi, I've been following the manual STM32-MAT/TARGET Hands On Rev 2.2 (see attached) and I am not able to get the timer 1 working (everything is working except this). I did everything like in the manual but when I load the .ioc file into simulink I get the next error:

 

### TIMERS_Config function : Can not find which APB timer TIM1 is connected to.Default preference value STM32TIMAPB set to APB1 is used.

 

I am using the STM32F767ZI nucleo.

 

Anybody knows how to solve this issue? Am I missing something?

 

Thanks in advance!

Attachments

Outcomes