AnsweredAssumed Answered

GPIO state at power down

Question asked by Lukasz Przenioslo on Feb 3, 2018
Latest reply on Feb 5, 2018 by Lukasz Przenioslo

Hello there,

According to the datasheet, the GPIO ports circuit diagram looks like this in STM323L4x2:

 

 

From this diagram I understand that at powerdown (VCC = VSS = 0 V) the I/O pin state is high impedance. But is that 100% correct? I want to make sure before I make a design move that would save me some components. But for this I need to know either there are no internal pull-downs on a pin when the MCU is powered down.

I would appreciate all help.

Outcomes