AnsweredAssumed Answered

LIS3DH with strange output values

Question asked by Rafael Costa on Feb 2, 2018
Latest reply on Feb 7, 2018 by Rafael Costa

Dear all,

    

   For one important project i need to detect the human falls. I am using the LIS3DH accelerometer configured as the following manner:  

 

        CTRL_REG1=0x77 //ODR=400 Hz, high-resolution mode/normal mode, ZYX axis enabled

        CTRL_REG2=0x01 // High pass filter enabled for AOI function on interrupt 1

        CTRL_REG3=0x40 // IA1 interrupt on INT1

        CTRL_REG4=0x84 // Output register not updated until MSB and LSB reading, high-resolution enabled

        INT1_THS=0x20      // 16mgx32=0,512g

        INT1_CFG=0x2A     // Or combination of interrupt events. Enable interrupt generation on X, Y and Z high event.

 

When the accelerometer has just the gravity acceleration applied along the z-axis, the output registers OUT_X_L, OUT_X_H, OUT_Y_L, OUT_Y_H, OUT_Z_L have the value 0, the register OUT_Z_H has the value 255.

 

When i apply acceleration the output registers OUT_X_L,OUT_X_H,OUT_Y_L,OUT_Y_H,OUT_Z_L just assume one of the following values: 64;128,192. The register OUT_Z_H have always the value 255. Obviously the values should vary between 0 and 255. When i apply acceleration is generated one interrupt on the pin INT1 detected by one microcontroller. On attachment i send the values of the output registers and the calculated acceleration.

 

Any help will be very appreciated.

Best regards,

Rafael Costa

Attachments

Outcomes