AnsweredAssumed Answered

Motor Control Libary on STM32F107 CL device

Question asked by evans.luke on Mar 28, 2014
Latest reply on Mar 31, 2014 by Gigi
Hi
I am running the Motor Control library 3.4.1 on the STM32F107xC.
It keeps crashing into the 'Hardware Fault' exception.
I have made the necessary adjustments to the IAR project build, and had to adjust some defines in the library to extend the build configuration past the STM32F10X_HD.
Is there some basal reason that the library is not documented to run on the F107 device?
Or, what could be throwing the hardware exception?
Thanks
Luke

Outcomes