AnsweredAssumed Answered

X-NUCLEO-IDB04A1 with Nucleo STM32F103

Question asked by M Greally on Jan 31, 2018
Latest reply on Feb 12, 2018 by M Greally

Hi.

 

I am using the  X-NUCLEO-IDB04A1 with Nucleo STM32F103 and the available demos are only for F4, L0 and L4. This is fine as I want to learn about programming bluetooth anyway. The BLUENRG chip on the expansion board is also a MCU and can be programmed. 

 

My question is: Do I need to program both devices and if so how, or can I treat the BLUENRG as a simple peripheral and control with standard SPI? Does the BLUENRG need to be programmed or is that only when using it as an MCU?

 

Thanks.

 

M.

Outcomes