AnsweredAssumed Answered

STC3115 Adjusting Configuration

Question asked by Chip Weller on Jan 30, 2018

After reading the STC3115 datasheet (D023755 Rev 8) and system integration (AN4324), plus FAQ and the driver code on GitHub, I have questions about the REG_VM_CFG, REG_CC_CFG, REG_VM_ADJ and REG_CC_ADJ.

 

Are the *_CFG parameters automatically updated by the IC?

If not, is there an algorithm I should used to adjust them with the *_ADJ registers?

 

Thanks

Outcomes