AnsweredAssumed Answered

Motor Control Serial Interface - Change USART for MCWB

Question asked by evans.luke on Mar 25, 2014
Latest reply on Mar 31, 2014 by Gigi
Hi
The motor control SDK 3.4 provides me with an LCDProject, which I believe contains the binary for the communications interface to the Motor Control Workbench program.
There doesn't seem to be any source code provided for this feature, and the MCWB program seems to offer no options for nominating the MCU USART or UART for use with that feature.

Is there a way to customise that feature to use a different MCU USART/UART peripheral, or are we stuck with USART1?

Thanks
Luke

Outcomes