AnsweredAssumed Answered

Comparator in STM32F373?

Question asked by Charles on Jan 19, 2018

Hello i have any question about Comp in STM32F3

1. What is the propagation delay for low overdrive, for example 5mV? In DS is only for 100mV. For High speed mode.

2. What is the output current for Low and high level on output commparatar?

3. What is the large-signal differential voltage amplification?

4. If is used internal DAC for driving one comparator input, can be used DAC without buffer?

 

Outcomes