AnsweredAssumed Answered

STM34CubeMX does not start

Question asked by baecklund.per on Oct 20, 2014
Latest reply on Nov 19, 2014 by qwer.asdf
I had CubeMX installed and working fine. Then I updated the application and now all I see is dialog flashing by the says "Check files". After that nothing happens.
When I start it from a DOS box I get:
java -jar STM32CubeMX.exe
HeapMemory: 16252928
Using Application install path:C:\Program Files\STMicroelectronics\STM32Cube\STM
32CubeMX
Using Application install path:C:\Program Files\STMicroelectronics\STM32Cube\STM
32CubeMX
loadPluginJar : clock
loadPluginJar : add clock
loadPluginJar : filemanager
loadPluginJar : add filemanager
loadPluginJar : ipmanager
loadPluginJar : add ipmanager
loadPluginJar : pinoutconfig
InternalPropertyChange: ChangeKeepUser  dont care
loadPluginJar : add pinoutconfig
loadPluginJar : power
loadPluginJar : add power
loadPluginJar : projectmanager
This is Windows
This is 32 Bit VM
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\\db\plugins\projectman
ager\windows\32\toolgen.dll
loadPluginJar : add projectmanager
loadPluginJar : updater
Using Application install path:C:\Program Files\STMicroelectronics\STM32Cube\STM
32CubeMX
STM32CubeMX Software Update Start Now

I have reinstalled the program with the same result.
Suggestions?

Outcomes