AnsweredAssumed Answered

CubeMX 4.4.0 unexpected behavior

Question asked by Dario_D on Oct 20, 2014
Latest reply on Nov 12, 2014 by STM32Cube-T
Hi all,
Yesterday I tried to align my project developed with CubeMX 4.3.1 to the recent 4.4.0 version.
I did itmainly to overcome a SysTickInit issue with FreeRTOS configuration.
Since the regenerated project compiles but won't start, I noticed the following error:
Generating a project using the attached file with CubeMX 4.3.1 will generate a correct main.c file.
Generating a project using the attached file with CubeMX 4.4.0 will generate a main.c file in which all the MX_XXXX_Init(void) routines do not contain the related HAL_XXXX_Init(&yyyy) function call.

Can someoneexplainthis behavior?
Thanks in advance to anyone.

Dario

Attachments

Outcomes