AnsweredAssumed Answered

EEPROM Emulation for the STM32 CubeF1

Question asked by Mathias Giacomuzzi on Jan 17, 2018
Latest reply on Jan 18, 2018 by Mathias Giacomuzzi

Hi,

 

In the STM32Cube_FW_F1_V1.6.0 software package i found the EEPROM example. STM32Cube_FW_F1_V1.6.0\Projects\STM32F103RB-Nucleo\Applications\EEPROM

Can someone tell me how the flash reservation is handle here? How big is the EEPROM and where can I decide how many pages are used for that?

 

I do not know how the pages are handled so that the user code is not flashed into the EEPROM pages because when I looked at the linker script I do not found anything different to a standard linker file. For me it is strange why there isn´t any extra Memory Area reservation for the EEPROM or some other reservation over sections or so.

 

Many thanks

mathias

Outcomes