AnsweredAssumed Answered

Nucleo-L152RE  + CubeExpansion_MEMS1 + Keil error

Question asked by Soham Jani on Jan 10, 2018

I'm trying to build an example project that comes with the "STM32CubeExpansion_MEMS1_V4.2.0" using Keil. 

It shows the following error: 

startup_stm32l152xe.s: error: A1023E: File "..\..\..\..\..\..\..\Drivers\CMSIS\Device\ST\STM32L1xx\Source\Templates\arm\startup_stm32l152xe.s" could not be opened: No such file or directory 

 

I'm using X-NUCLEO-IKSO1A1 expansion board. 

Other examples that come with STM32Cube library build and flash fine. (Eg Blnky)

 

Would love some help figuring this out. Thanks 

Outcomes