Philipp Krause

3rd Feb talk on The free toolchain for the STM8 at FOSDEM in Brussels

Discussion created by Philipp Krause on Jan 9, 2018

At FOSDEM 2018, there will be a talk on "The free toolchain for the STM8" in the "Embedded, mobile and automotive devroom".

 

The talk in the will be 2018-02-03 11:00 in room UD2.218A at the Université libre de Bruxelles.

 

There has been a lot of recent progress, from the speed optimizations in SDCC to the on-target-debugging support via OpenOCD and GDB.
I will also be around for discussions during that weekend.

 

More details on the talk can be found at:
https://fosdem.org/2018/schedule/event/the_free_toolchain_for_the_stm8/

 

Philipp

Outcomes