AnsweredAssumed Answered

run motor without the use of st motor control workbench

Question asked by Low Yik Seong jordan on Jan 8, 2018
Latest reply on Jan 9, 2018 by Erwan Y

Hi, I am trying to modify the the code which is compiled from st motor control workbench. So far i have successfully run using st motor control workbench. May I ask is it possible to modify the code so that it does not need to run through the st motor control workbench which include adjusting the speed of motor just by varying the potential-meter on motor driver. If it is possible, which document do I need to refer to? Thanks

Outcomes