AnsweredAssumed Answered

Keil Configuration Wizard - Doesn't Accept Decimal Point Numbers

Question asked by cooke.ernest on Jan 4, 2018
Latest reply on Jan 4, 2018 by Clive One

Hi,

 

I have just started working on a configuration wizard utility in Keil uVision for the setup of stepper motors.

 

As can be seen, the configuration wizard so far setups the acceleration, deceleration, maximum and minimum speed etc. of the motor just fine.

 

However, for the distance per step option I would like to use a decimal point number, say 9.4 mm per step.  However the configuration wizard is not allowing me to enter decimal point numbers.

 

Is this a limitation of the configuration wizard or is there a method of entering decimal point numbers?

 

Any answers are greatly appreciated.

 

Thanks,

Ernest

 

 

Outcomes