AnsweredAssumed Answered

dSPIN Evaluation Software control two motors with separate chip selects

Question asked by jarratt.robert on Jan 28, 2014
Latest reply on Mar 11, 2014 by Gigi
Hi,
I have an SPEVAL-PCC009V2 with EVAL-6470H setup controlling one stepper motor very effectively.  I want to control two motors but would prefer to do this using separate chip selects for each L6470 instead of using the daisy chain configuration described in AN3991.  Is is possible to do this?

Possibly related to the above question, is is possible to extend the scripting language in dSPIN to include control of additional IO ports in the STEVAL-PCC009V2?

Thanks,
Bob

Outcomes