AnsweredAssumed Answered

Adding the I-CUBE-LRWAN library to a STM32CubeMX project

Question asked by Alexandre Jamet on Jan 2, 2018
Latest reply on Jan 19, 2018 by Andrew Neil

My team and I are currently working on a project that involve a ST board (the STM32L072CZYxx) to create a bidirectionnal GSM-LoRa gateway.

As we've already succeeded in implementing the GSM side of the gateway, we are currently working on the LoRa part of the project. To achieve this, we're trying to use the I-CUBE-LRWAN, but can't figure out how to add this library to the STM32CubeMX project. It seems like, this library can't be added to our project through STM32CubeMX. The only solution we have is to add manually the library to the project but we can't figure out how to do it. We imported the middlewares we needed into the project however, the IDE we use (Atollic TRUEStudio or SW4STM32) detects a lot of errors in the project and we really don't understand why (the source for middlewares were coded by ST, so basically no errors).

Outcomes