AnsweredAssumed Answered

Compile time is taking forever

Question asked by b.m.002 on Dec 18, 2017

Hi Everyone.

I recently updated my SW4STM32 IDE when prompted to do so from a pop up, and I'm now seeing its taking forever to compile a project. For example I cleaned one of my STM32F0 Adafruit LCD shield demo programs and then rebuilt it with the following stats finally displayed via the console view.

 

06:07:06 Build Finished (took 1m:46s.283ms), this is forever?

 

It was going through building each file one by one taking at least a second or so on each file. Is this something someone else is experiencing, can I fix this somehow?

 

EDIT: Also making a trivial code change produced this.

06:20:51 Build Finished (took 4s.363ms)

 

Thanks

mb

Outcomes