AnsweredAssumed Answered

First Time Connection SPWF04SA - Faild   ,please help

Question asked by maor.yaniv.001 on Dec 12, 2017
Latest reply on Dec 14, 2017 by Mridupawan Das

Hello running the example code  : WIFI_Example_Client_Socket

 

using SPWF04SA

 

also the server program in the st utility ip 10.0.0.1 (checked with external socket.exe and worekd)

 

 

but the WIFI_Example_Client_Socket  moo working or sending data please view the log...

 

/********************************************************

 

 

*                                                      *

 

 

* X-CUBE-WIFI1 Expansion Software v3.1.0               *

 

 

* X-NUCLEO-IDW0xx1 Wi-Fi Configuration.                *

 

 

* Client-Socket Example                                *

 

 

*                                                      *

 

 

*******************************************************/

 

 

Do you want to setup SSID?(y/n):y

 

 

Enter the SSID:

yaniv

 

 

Enter the password:

magic111

 

 

Enter the encryption mode(0:Open, 1:WEP, 2:WPA2/WPA2-Personal):

2

 

 

Enter the Hostname (Apache Server):

10.0.0.1

 

 

 

 

 

 

/**************************************************************

 

 

* Configuration Complete                                     *

 

 

* Port Number:32000, Protocol: TCP/IP                        *

 

 

* Please make sure a server is listening at given hostname   *

 

 

*************************************************************/

 

 

 

 

Initializing the wifi module...

 

 

Build Configuration:

Nucleo: NUCLEO-L476RG

X-Nucleo: X-NUCLEO-IDW04A1

Interface: UART

 

with the flowing setup :

 

then when it freeze / stoped

Outcomes