AnsweredAssumed Answered

SPWF04Sx - WebServer - HTTP

Question asked by yoann LBY on Dec 11, 2017
Latest reply on Dec 11, 2017 by Gerardo Gallucci

hi,

is it possible to limit a connection to the module with one client?

wifi module is miniAP mode and HTTP server application run with web pages html.

One client connect to the wifi module

+WIND:28:Station Associated:44:85:00:F8:B6:DC:0

and i don't want a second client to connect in the same time of client1.

+WIND:28:Station Associated:08:11:96:9D:5E:D8:0

 

thks

Yoann

Outcomes