AnsweredAssumed Answered

STBC03 Eval Kit Manual (and Board?) Error

Question asked by Scott Deyo on Dec 11, 2017

In the STEVAL-ISB035V1 Manual (UM2132), the schematic and ball-out refer to the STBC02 instead of the -03.

Also, on the board, both R11 (in the "02" section") and R8/ R13 (in the "03" section) are installed. This doesn't seem right, since BATMS_EN should be high or low, not divided.

A hyperlink in datasheets would be useful for reporting mistakes.

Outcomes