AnsweredAssumed Answered

I need the driver for the EVALKITST8500-1 evaluation kit (Windows 7)

Question asked by Sameer Damir on Dec 8, 2017

I cant connect to my EVALKITST8500-1 using Smartgrid LabTool V4.4.The power cable and the USB cable for kit interface are connected properly. When I connect the interface cable as per the the quick start guide, the LabTool does not recognize any port.
If I go to settings - port: I can find no port to choose
If I go to settings - COM port - Scan port: Again, nothing happens.
In my windows device manager, I can see two new devices which don't have the appropriate driver, there are named: Enhanced COM port, and standard COM port.

Outcomes