AnsweredAssumed Answered

SW enter HardFault_Handler using OpenStm32

Question asked by kent gu on Dec 1, 2017
Latest reply on Dec 1, 2017 by Clive One

Hi,

The project is developed with Keil MDK, it run well. But I use OpenStm32 to create one project, and copy the source code into the OpenStm32 project. I can run with ST Jlink V2, but the code enter HardFault_Handler while run "TIM_Cmd(TIM4,ENABLE); ". 

 

BTW, I use old stm32f10x_it.c (V3.3.0) version,other driver file are old version.

 

 

Best Regards,

Kent

Outcomes