AnsweredAssumed Answered

ST Link External Loader Not Recognized

Question asked by paye.corey on Dec 1, 2017
Latest reply on Dec 6, 2017 by Clive One

Hello,

I am using the ST-Link utility, v4.0.0.  I created a custom external loader in IAR for ARM using one of the example projects.  After I build the loader in IAR I copy the .out file to ST Link's external loader folder and give it an STLDR extension.  However when I go to load the file through ST Link, the Device name is blank, the Device Type is "Unknown Device, the Start address is 0 and the Device Size is 0.  I know that this information comes from the Dev_Inf file but since I just modified an existing project, I think this is all setup correctly.  I have built this both in IAR v7.3 and v7.8.  Any guidance would be appreciated.

 

Thanks.

Outcomes