AnsweredAssumed Answered

ADC Voltage reference doubt

Question asked by Sergi Hernandez on Nov 30, 2017
Latest reply on Nov 30, 2017 by waclawek.jan

Hi, 

 

I'm working with a STM32L053R8 and I want to use some ADC pins. I have a doubt about the input voltage range. 

 

Does the ADC have an independent power supply? 

Which is the input voltage range of the ADC?

 

For example:

 

Let's suppose that I am supplying the STM with 3.3 V, and I am using 12 bits from the ADC.

 

That means that...?

 

- The input voltage range goes from 0V to 3.3V?

- The step-quantization is 3.3/(2^12-1)?

 

 

Thanks!  

Outcomes