AnsweredAssumed Answered

ST Link Utility : the elf loader is bigger than the ram size

Question asked by Thomas Lotz on Nov 24, 2017
Latest reply on Nov 27, 2017 by Thomas Lotz

Hello,

 

When I try to erase chip (STM32L011F4U6) with ST Link utility, it do not works and I get the message "the elf loader is bigger than the ram size", see the enclosed picture.

 

I use the ST Link side of a NUCLEO-L053R8 board connected to a cutom board with the STM32L011F4U6.

St link connection is ok, and I'm able to read the device memory, so the hardware SWD connection seems to work well.

 

FYI : when I try to debug the STM32L011F4U6 from the development environment System Workbench for STM32, it does not work either.

 

I hope you can help me find a solution

Thanks !

 

Thomas

Attachments

Outcomes